AnsweredAssumed Answered

STM32F746G-DISCO - fail RESERVED BITS when copy bin from mbed

Question asked by karol.karol on Jun 28, 2016
Latest reply on Jun 29, 2016 by Clive One
Hi, I have a problem with my stm32f46g disco board. When I want to compile program on mbed.org and after that copy that file to disco board I get a fail.txt and info: RESERVED BITS. What happen? I may connect with ST-Link, its connects without problem.

09:48:33 : ST-LINK SN : 066AFF525053885087033137
09:48:33 : ST-LINK Firmware version : V2J23M7
09:48:33 : Connected via SWD.
09:48:33 : SWD Frequency = 1,8 MHz.
09:48:33 : Connection mode : Normal.
09:48:33 : Device ID:0x449
09:48:33 : Device family :STM32F7xx

fail.png

Outcomes