AnsweredAssumed Answered

STM32F107 - mass storage device

Question asked by rifo.rifo on Jun 17, 2016
Latest reply on Jun 26, 2016 by rifo.rifo
Hello,

I am planning to build a device with a STM32F107, The user should be able connect to the system via both Ethernet and USB.

When connected via ethernet, I should inform the IP address of STM32F107 to the user.

For this I thought about the following, can you please comment if this is possible?

When the user plugs in the USB cable, my device will act as a Mass storage device and pop up as a folder.
In the folder, a txt file will be shown, an STM32F107 will write the IP address it gets in this txt file

Can you please guide me about how to implement this scenario?

thanks a lot
rifo

Outcomes