AnsweredAssumed Answered

is BOOT pin needed for IAP of new firmware

Question asked by rifo.rifo on Jun 17, 2016
Latest reply on Jun 19, 2016 by rifo.rifo
Hello,

I am designing a board with a STM32F0308.

STM32F0308 will be connected to a linux based SOC via UART connection. When a software update is required, I plan to send the new firmware for STM32F0308 via uart and then store it in external nand/nor flash.

After the firmware is acquired, I want to update STM32F0308 internal flash and then start with the new bootloader.

My question is, during this process, can you please confirm that I don't need to use BOOT pin?   

thanks
rifo

Outcomes