AnsweredAssumed Answered

DFU standalone doesn't work

Question asked by bruno.vincenzo on Jun 10, 2016
Latest reply on Jun 10, 2016 by bruno.vincenzo
I use IAR EW 7.1, HAL driver and STM3210E_EVAL.
I would use the application DFU and like user application CDC_standalone.
I've used like configuration for CDC_standalone
#define VECT_TAB_OFFSET  0x7000
and  I'm changed the value in the Linker of the Vector Table in 0x08007000
and range of ROM, start is 0x08007000 and end is 0x08080000.
This, because in DFU application is defined
 
/* Test if user code is programmed starting from address 0x08007000 */
   if (((*(__IO uint32_t*)USBD_DFU_APP_DEFAULT_ADD) & 0x2FFE0000 ) == 0x20000000)
   {
     /* Jump to user application */
     JumpAddress = *(__IO uint32_t*) (USBD_DFU_APP_DEFAULT_ADD + 4);
     JumpToApplication = (pFunction) JumpAddress;
      
     /* Initialize user application's Stack Pointer */
     __set_MSP(*(__IO uint32_t*) USBD_DFU_APP_DEFAULT_ADD);
     JumpToApplication();
   }
 }
and is defined 
#define USBD_DFU_APP_DEFAULT_ADD               0x08005000 /* Start user code address: ADDR_FLASH_PAGE_10 */
#define USBD_DFU_APP_END_ADD                   0x080FF800 /* Start address of latest flash page: ADDR_FLASH_PAGE_511 */

I've generated file.bin for DFU file manager.
I've used
VENDOR ID 0x0483
Product ID 0xDF11
as defined in DFU application
#define USBD_VID                      0x0483
#define USBD_PID                      0xDF11

I've used Target ID 00 and as Address start in Multi Bin injection 08007000, thus I've generated file.dfu.
So, with DFUSEDemo I've upgrade file.dfu on board.
But does't work.
Thank's a lot for your advices.

Outcomes