AnsweredAssumed Answered

IAP Go to infinite loop when Hard Fault

Question asked by bruno.vincenzo on Jun 8, 2016
Latest reply on Jun 9, 2016 by bruno.vincenzo
STM3210E_EVAL on board after erasing the flash, I installed IAP application as STM32Cube_FW_F1_V1.3.0.
Running the IAP program without having loaded any user application code, the micro goes hard fault. I think it is normal.
After I tried to load the bin file obtained by compiling the application CDC_Standalone as applicatione user.
But the micro is still hard fault.
What am I doing wrong?
The generated bin file of the sample file?
I'm using the STM32Cube_FW_F1_V1.3.0 applications.

Outcomes