AnsweredAssumed Answered

Which parameters are suitable for aci_hal_set_tx_power_level with SPBTLE-RF ?

Question asked by JulienD on Aug 4, 2016
Latest reply on May 14, 2018 by Scott Lohr
Hi,

The description in the .h file states that:
"
 * @param en_high_power Can be only 0 or 1. Set high power bit on or off. It is strongly adviced to use the
 *                         right value, depending on the selected hardware configuration for the RF network:
 *                         normal mode or high power mode.
"

So, which value should be used as en _high_power with the SPBTLE-RF module?

Thanks
Julien

Outcomes