AnsweredAssumed Answered

STM32F469I-Disco CAN Interfaces connections

Question asked by Karadimitriou.Nikola on May 19, 2016
Latest reply on May 20, 2016 by Karadimitriou.Nikola
Hi, I have successfully connected and run the CAN2 interface on this board.
Now,
 I'm trying to connect the CAN1 but I can not find the corresponding port pins on the board. I've been reading the pds but there is no information on the CAN1 interface. Only the CAN2 which is set up through the EXT connector. 

I have configured the CAN1 to be on PA11->RX and PA12->TX.
Does anyone know which are these ports on the actual board? 

Thanks in advance.

Outcomes