AnsweredAssumed Answered

TIM PWM input mode

Question asked by obid.matic on May 17, 2016
Latest reply on May 17, 2016 by Clive One
Hi.

I would like to use PWM input mode on a TIM1. PWM signal on my custom PCB is connected to TIM1 channel 4. Now, I figured out that CubeMX allows to configure PWM input mode only, if PWM signal is connected to channel 1 or 2. Thus, CNT values would be captured in CCR1 and CCR2 registers.

I am asking, if it is also possible to connect channel 4 and channel 3 to PWM input mode? Ref. manual doesn't explicitly say that this combination could not be configured. Any idea?

Edit: I already found out in other topics that PWM input mode is possible only on CH1 and CH2.

Thanks

Outcomes