AnsweredAssumed Answered

Error when using __attribute__((at(address))) for data definition

Question asked by obid.matic on May 16, 2016
Latest reply on May 16, 2016 by Clive One
Hi.

I tried to use __attribute__((at(address))) to define a global variable at certain address and Keil returned error L6971E, which is described here 

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0496c/CJAIGFIC.html


I don't really understand what is wrong, because if I use address at the beginning of RAM (let say 0x20000020) the error occurs, but if I use higher address (let say 0x20002000), the error doesn't occur.

Could anyone please explain what is wrong here and is it just OK if I define higher address, which is not causing an error?

Secondly, do I have to be aware of data alignment when using __attribute__((at(address)))?
I mean, do I have to use only 0x.......0, 0x.......4, 0x.......8, ... addresses for integers, only 0x.......0, 0x.......2, 0x.......4,  0x.......6, 0x.......8, ... addresses for half-word and any kind of address for bytes?


Thanks a lot.

Outcomes