AnsweredAssumed Answered

Resistive touch screen wrong coordinates

Question asked by Baev.Alexander on May 12, 2016
Latest reply on May 16, 2016 by Baev.Alexander

Hi.

I have a problem withresistive TP.

I use STMPE811.

I use my custom board with connection of the stmpe811 similar to the stm32f429discovery board, as well as the drivers from the board demonstration software.

I cannot get correctvalues of x and y.

To isolate the problem I take the values of x and y immediately after this function –stmpe811_TS_GetXY(...) and print them to the screen. The values are quite unstable. For example when I push in some part of the screen I receive something like this x = 1230, y = 3457. Holding the finger in the same spot the values of x and y change slightly (+-50) but once in 2-3 seconds those values are something absolutely different like x= 60, y = 6354234.

Another problem is when I move finger along the x axis the value of y also changes by several times (but it should stay the same as I don't change y position).

I tried to change touch detect delay, average control samples – the problem had notchanged.

Just for reference hereare the values of the corners:

       
  1.    

    left upper x = 2720,    y = 3500

       
  2.    
  3.    

    left lower x = 1900,    y = 4300

       
  4.    
  5.    

    right upper x = 4020,    y = 3600

       
  6.    
  7.    

    right lower x = 530,    y = 52014

       
  8.    
  9.    

    middle of the screen    x = 3670, y = 2180

       

As I mentioned the values are something absoultely different once per 2-3 seconds.

Is there something I can check?

Thanks.

Outcomes