AnsweredAssumed Answered

F107 USB OTG as a device only

Question asked by Wood.Robert on May 5, 2016
Latest reply on May 12, 2016 by Wood.Robert
Folks,

I have code for using the F103's USB device port as a virtual com port. Does anyone know:

1. Could I use that "as is" on the F107's OTG port. I only ever want to use it as a device.
2. Do I really have to have  OTG_FS_VBUS connected to the USB connector's 5V line? Sadly, the board's been laid out with PA9 - which is the VBUS connector - as the USART function.

Thanks!

Rob

Outcomes