AnsweredAssumed Answered

STM32F4 CAN HAL library - TX and RX

Question asked by pavone.alessandro on Apr 26, 2016
Latest reply on Apr 27, 2016 by pavone.alessandro
Hi,
I am using the STM32F429ZI CAN peripheral in polling TX and interrupt RX with HAL library V1.4.4 of 22-January-2016. This the procedure that I use:
       
  • During CAN init, I call the HAL_CAN_Receive_IT to enable the first receive interrupt;
  •    
  • At the end of my HAL_CAN_RxCpltCallback implementation, I call the HAL_CAN_Receive_IT to enable the next receive interrupt;
  •    
  • Every 100ms in the main I call a HAL_CAN_Transmit.

Here my problem: sometimes the receive interrupt occours during HAL_CAN_Transmit execution where CAN peripheral is locked (__HAL_LOCK(hcan);). In this case the receive interrupt return a BUSY without end the receive procedure and without call the HAL_CAN_RxCpltCallback, so I can not receive other message!

Do you have some suggestion to solve this problem??

Inside HAL_CAN_Receive_IT I tried to comment the line __HAL_LOCK(hcan); e
 __HAL_UNLOCK(hcan); and all is ok. This solution in my opinion is not good.

Thank you very much.
Alex





Outcomes