AnsweredAssumed Answered

Flash program error when using fast mode

Question asked by abid.hassan.001 on Apr 22, 2016
Hi, 
   I am trying to use the fast program method to write a row (256 bytes) to the flash. But when HAL_Flash_Program() function is called, the PGAERR flag is raised. The input buffer as well as the write address are 256 byte aligned.

Outcomes