AnsweredAssumed Answered

FreeRTOS and BSP Drivers ST32L152D-EvalBoard STM32CubeL1

Question asked by oltean.andreea on Apr 22, 2016
Hello,

I want to integrate the FreeRTOS and the BSP drivers in the same project for the ST32L152D-EvalBoard. I am doing my project in Atollic TrueSTUDIO and I am using the code from STM32CubeL1.
Is there an easy way to do that: should I start with the FreeRTOS application and add the drivers on top, or should I start with e.g. the LCD example, and then include the FreeRTOS files?
Thank you! Any idea would help me!

Outcomes