AnsweredAssumed Answered

USB HOST (type A) advice

Question asked by prieur.jean on Apr 6, 2016
Latest reply on Apr 11, 2016 by Quentin
Hello everybody!

I want a little advice on the best way to code (on a STM32F4) an USB HOST "ONLY" with a standard type A connector.

The picture of the STM32 > USB CONNECTOR cabling is attached: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/65016/USB_HOST.jpg

I already coded in the past an USB SLAVE (with a midi USB connector), using the library STM32_USB_OTG_Driver

Now I want to start a new project and create an USB HOST, to host and communicate with my USB SLAVE circuit.

So my questions are:
1) Is the system on the picture attached is correct?
2) To configure the USB host driver, I need to use the USB OTG HS CONFIGURATION instead of the USB OTG FS CONFIGURATION ?

Thanks a lot, have a good day!

Attachments

Outcomes