AnsweredAssumed Answered

FSMC external RAM in DMA mode

Question asked by Mazzetti.Francesco on Mar 21, 2016
Latest reply on Mar 21, 2016 by Mazzetti.Francesco
Hello
First to start to develop my new application I need some answers from someone that know FSMC in external RAM mode.

1) Can I consider the external RAM like internal? (using linkerScript.ld??)
2) Is it possibile write in DMA peripheral to memory mode without prebuffer in "normal" RAM?
3) And If I have two simultaneous circular DMA pherip-to-mem while I reading some variable under interrupt? The FSMC controller can manage this condition? (multi read/write)

Thanks!!!!!

Outcomes