AnsweredAssumed Answered

My first STM32 based circuit, is this circuit ok?

Question asked by gould.terry on Mar 18, 2016
Latest reply on Mar 28, 2016 by Amel N
Hi,
This is my first time working away from Arduino.

I am creating a simple CAN bus analyser using a STM32F105RBT6

I have used parts of circuits from various evaluation boards. 

But I am mainly concerned about the Power circuit. I want to be able to power from VIN or USB. Both are to be able to be powered at the same time.

I have also seen similar circuits using a 8mhz or 25mhz so I am not sure which to use.

The Image dialog on here doesn't seem to work on Safari or Chrome on Mac so please check out this post:

http://electronics.stackexchange.com/questions/215097/is-this-stm32f-based-can-bus-circuit-ok


Outcomes