AnsweredAssumed Answered

STM32CubeMX V4.3 & Keil MDK 4.7 linking problem

Question asked by Osto on Jul 20, 2014
Latest reply on Aug 14, 2014 by Osto
Hi,

When I make Project, generate code, open Project in MDK, Close NKD, Change Project, generate again, open MDK,....... several times then following happens:

1.) every 2,3,4th times, when I build all of MDK Project, I get following message:
ControllerV2 Configuration\ControllerV2 Configuration.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST.
Keil says that this means that there is no main function available. How ca this happen?

2.) Every time I generate the Project in CubeMX then 3 new lines added to my include path in C/C++ configuration. So after 5 time generate, I have ~20 entries in C/C++ include path in the Project configuration. How can I fix that without every time to delete all addede entries.

3.) After every generate,  a lot of entries in my MDK Project configuration are changed. For example my Quarz freqencies, type of Emulator, type of Debug,.... How can I hint the CubeMX from changing These values?

I Need o say that this tool is the best tool I had in the last 5 years. It helps me to save huge amount of time to configure the contoller for the required Outputs.

Thanks a lot

Outcomes