AnsweredAssumed Answered

F103ZET6 CAN on PB8 and PB9

Question asked by Bartocha.Mateusz.001 on Mar 3, 2016
Latest reply on Mar 7, 2016 by Bartocha.Mateusz.001
Hello!

I have a problem with stm32 F103ZET6 and CAN on alternate pinout - PB8 and PB9.

I created a project using CubeMX, set PB8 and PB9 for can functionality, generated code and put it into Keil.

Below you can find my main.c code.

/**
  ******************************************************************************
  * File Name          : main.c
  * Description        : Main program body
  ******************************************************************************
  *
  * COPYRIGHT(c) 2016 STMicroelectronics
  *
  * Redistribution and use in source and binary forms, with or without modification,
  * are permitted provided that the following conditions are met:
  *   1. Redistributions of source code must retain the above copyright notice,
  *      this list of conditions and the following disclaimer.
  *   2. Redistributions in binary form must reproduce the above copyright notice,
  *      this list of conditions and the following disclaimer in the documentation
  *      and/or other materials provided with the distribution.
  *   3. Neither the name of STMicroelectronics nor the names of its contributors
  *      may be used to endorse or promote products derived from this software
  *      without specific prior written permission.
  *
  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
  * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
  * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
  * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
  * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
  * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
  * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
  *
  ******************************************************************************
  */
/* Includes ------------------------------------------------------------------*/
#include "stm32f1xx_hal.h"
 
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan;
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN_Init(void);
 
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
 
/* USER CODE END PFP */
 
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
int main(void)
{
 
  /* USER CODE BEGIN 1 */
 
  /* USER CODE END 1 */
 
  /* MCU Configuration----------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_CAN_Init();
 
  /* USER CODE BEGIN 2 */
 
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
     
    CanTxMsgTypeDef TxMess;
     
    TxMess.StdId = 0x123;
  TxMess.DLC = 0x0;
  TxMess.Data[0] = 0x12;
  TxMess.IDE = 0;
  TxMess.RTR = 0;
     
    hcan.pTxMsg = &TxMess;
  while (1)
  {
  /* USER CODE END WHILE */
         
        HAL_CAN_Transmit(&hcan, 100);
         
        HAL_Delay(200);
 
  /* USER CODE BEGIN 3 */
 
  }
  /* USER CODE END 3 */
 
}
 
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
 
  RCC_OscInitTypeDef RCC_OscInitStruct;
  RCC_ClkInitTypeDef RCC_ClkInitStruct;
 
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = 16;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  HAL_RCC_OscConfig(&RCC_OscInitStruct);
 
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
  HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
 
  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
  /* SysTick_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
 
/* CAN init function */
void MX_CAN_Init(void)
{
 
  hcan.Instance = CAN1;
  hcan.Init.Prescaler = 16;
  hcan.Init.Mode = CAN_MODE_NORMAL;
  hcan.Init.SJW = CAN_SJW_1TQ;
  hcan.Init.BS1 = CAN_BS1_1TQ;
  hcan.Init.BS2 = CAN_BS2_1TQ;
  hcan.Init.TTCM = DISABLE;
  hcan.Init.ABOM = DISABLE;
  hcan.Init.AWUM = DISABLE;
  hcan.Init.NART = DISABLE;
  hcan.Init.RFLM = DISABLE;
  hcan.Init.TXFP = DISABLE;
  HAL_CAN_Init(&hcan);
 
}
 
/** Pinout Configuration
*/
void MX_GPIO_Init(void)
{
 
  /* GPIO Ports Clock Enable */
  __GPIOB_CLK_ENABLE();
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
#ifdef USE_FULL_ASSERT
 
/**
   * @brief Reports the name of the source file and the source line number
   * where the assert_param error has occurred.
   * @param file: pointer to the source file name
   * @param line: assert_param error line source number
   * @retval None
   */
void assert_failed(uint8_t* file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
    ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
 
}
 
#endif
 
/**
  * @}
  */
 
/**
  * @}
*/
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/


The problem is that on CAN_H and CAL_L im able to se only high state. I've analyzed it with scope and also right on PB8 and PB9 I see high all the time.

I'm sure that that pins are not shorted to Vcc - I've performed a test to set those pins as digital output and toggled it every 100ms and I have seen proper state switching on scope.

Can you see any bug ? Maybe something is wrong with my micro.

Thanks for help.

Matthew

Outcomes