AnsweredAssumed Answered

This can be realized with DAC and ADC in STM32F103?

Question asked by cecil.werner on Mar 1, 2016
Latest reply on Mar 2, 2016 by AvaTar
DAC.png
DAC is used for generating sinus wave 1kHz.
1000 sample is over DMA transferred on DAC 1MHz/1000SPS = 1kHz
It would be good to start each sinusoid nullify one of the counters.
This signal, after passing through something DUT return on ADC

After generated fifty sinus wave is started ADC and over DMA make 1000 measure on 1MHz

What is the purpose?
Determine the attenuation and shift waves at DUT.
Rapidinsight intothe datasheetno problem,butratherask:

Outcomes