AnsweredAssumed Answered

using the fsmc to boot from NOR and run with pSRAM -MCP - STM32F439

Question asked by az.E on Feb 28, 2016
Latest reply on Feb 28, 2016 by Clive One
Hi.
I would like to understand wheather it is possible to use the FSMC of the STM32F439 to interface with a MCP module  - NOR FLASH+pSRAM, where the address and data are shared and multiplexed .
I see that there is a bank for NOR /PSRAM , but is it possible to work with both on the same chip ?
will it be possible to boot from the nor and run with the RAM after ? does the driver support address/data multiplexing ?
thank you !
Daniel

Outcomes