AnsweredAssumed Answered

Cortex M0 Non Volatile Memory Storage

Question asked by Johnson.Mark.001 on Feb 26, 2016
Latest reply on Jun 1, 2017 by Zhitai Liu
Is anyone aware of a method or even the feasibility to transfer captured data from the ADC module, transferred to SRAM, then stored to non volatile memory (flash) section of the Cortex M0 Arm core without having to externally store the data to another device?
Example: An application requires to count people walking through a doorway. This data can be easily acquired and stored in Cortex M0 SRAM. However if the system lost power or reset, the data is lost. The application would required to update the data every time a count occurred.
The data captured in SRAM would then need to be transferred to a non volatile (flash) area of the internal memory of the device.

Outcomes