AnsweredAssumed Answered

Uart Rx interrupt not working if clock for GPIOD is enabled

Question asked by yafis.mohamed on Feb 20, 2016
Hello.
I am using a custom board with STM32F030R8 as my dev platform. I am using Uart2 to configure the board. The RX interrupt is enabled to receive data. i am using PD2 as a GPIO.
When i enable peripheral clock to GPIOD, i am not getting uart rx interrupt but uart tx works fine. But when i do not enable the GPIOD peripheral clock everything works fine.
I have no idea what is the problem here...
Is there something i am missing here?

Outcomes