AnsweredAssumed Answered

Nucleo-F103 Reset not working.

Question asked by k.kvresto on Feb 5, 2016
Latest reply on Feb 6, 2016 by k.kvresto
Hi.
I have been programming my new nucleo_F103RB, a bit lately and I have noticed lately that when I program the micro with whatever I'm working on, the program finally runs after ST-LINK has finished. But when I disconnect my board from the USB port, and then  reconnect, nothing happens.

The code wont run, and I cannot I reset the micro with the reset switch. 
I think it might have something to do with mbed, because the only thing that happens when I reconnect is the explorer opens up and I can see an embed file stored on the device. 

Has anyone had this problem? can someone help out with a solution, or even an explanation as to why?

cheers

Outcomes