AnsweredAssumed Answered

Example for simple ADC conversion

Question asked by poseid on Jan 27, 2016
Latest reply on Jan 29, 2016 by tulip
Hello,

I am trying to get a simple example going for the ADC of an STM32F407V discovery board.

I tried the VBAT sampling example, but so far without luck. I only get "0,0" via serial port on the output.

My environment is based on CooCox, and I configure the clocks (f_sys) to run on 48 MHz with HSE 8 MHz. I use DMA to transfer data from the ADC to the main display function.

How can I start/debug the setup and experiment with the different ADC modes?

Thanks!

Outcomes