AnsweredAssumed Answered

FMC on STM32F4xx for Graphics Applications

Question asked by henry.blue on Jan 18, 2016
Latest reply on Jan 18, 2016 by Clive One
Hellos,
I see there is an inbuiltFMC on the STM32F4x9 MCUs which can interface to various memory types including NAND, NOR , SDR SDRAM. My question is: Is it a good idea to use the NOR or a NAND Flash as a FRAME buffer for graphics applications? If yes, which one of the below is a recommended choice for frame buffer to interface with the FMC.
1. NAND FLash
2.NOR FLash
3. SDR-SDRAM
4. PSRAM
5. 16-bit PC Cards

Outcomes