AnsweredAssumed Answered

CAN Bus - how do I set baud rate on STM32F303x?

Question asked by bigden.gary on Jan 14, 2016
Latest reply on Jan 14, 2016 by Clive One
The default examples are for the Discovery board running at 72MHz. Mine is running at 65.536MHz, meaning that I need to adjust the baudrate to get the round number I desire eg 1M, 500k, 250k, 125k etc.

It is not obvious from the s/w how I do this.

Outcomes