AnsweredAssumed Answered

STM32F072 usart doesn't reveive data

Question asked by tunder.pinyin on Jan 11, 2016
Latest reply on Jan 12, 2016 by FTITI.Walid
Hi,i am working with Stm32f072 microcontroller and i can send data successful.But my code doesn't enter usart interrupt.My code is below,thanks for your support.
void USART_Configuration()
{
    GPIO_InitTypeDef GPIO_Struct;
    USART_InitTypeDef USART_Struct;
    NVIC_InitTypeDef NVIC_Struct;
     
     
    /*USART1 Configuration*/
    RCC_AHBPeriphClockCmd(USART1_GPIO_Bus,ENABLE);
    RCC_APB1PeriphClockCmd(USART1_Bus,ENABLE);
     
    GPIO_PinAFConfig(USART1_GPIO_Port,USART2_GPIO_Pinsource1,USART1_Alternate);
    GPIO_PinAFConfig(USART1_GPIO_Port,USART2_GPIO_Pinsource2,USART1_Alternate);
     
     
     
    GPIO_Struct.GPIO_Pin=(USART1_Pin_Tx|USART1_Pin_Rx);
    GPIO_Struct.GPIO_Mode=GPIO_Mode_AF;
    GPIO_Struct.GPIO_OType=GPIO_OType_PP;
    GPIO_Struct.GPIO_PuPd=GPIO_PuPd_UP;
    GPIO_Struct.GPIO_Speed=GPIO_Speed_50MHz;
    GPIO_Init(USART1_GPIO_Port,&GPIO_Struct);
     
     
    USART_Struct.USART_Mode=((USART_Mode_Rx)|(USART_Mode_Tx));
    USART_Struct.USART_BaudRate=9600;
    USART_Struct.USART_WordLength=USART_WordLength_8b;
    USART_Struct.USART_Parity=USART_Parity_No;
    USART_Struct.USART_StopBits=USART_StopBits_1;
    USART_Struct.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
    USART_Init(USART1,&USART_Struct);
     
    USART_Cmd(USART1,ENABLE);
    /**************************************************************************/
     
     
     
     
    /*USART2 Configuration*/
    RCC_AHBPeriphClockCmd(USART2_GPIO_Bus,ENABLE);
    RCC_APB1PeriphClockCmd(USART2_Bus,ENABLE);
     
 
     
     
     
    GPIO_Struct.GPIO_Pin=(USART2_Pin_Rx|USART2_Pin_Tx);
    GPIO_Struct.GPIO_Mode=GPIO_Mode_AF;
    GPIO_Struct.GPIO_OType=GPIO_OType_PP;
    GPIO_Struct.GPIO_PuPd=GPIO_PuPd_UP;
    GPIO_Struct.GPIO_Speed=GPIO_Speed_50MHz;
    GPIO_Init(USART2_GPIO_Port,&GPIO_Struct);
     
    GPIO_PinAFConfig(USART2_GPIO_Port,USART2_GPIO_Pinsource1,USART2_Alternate);
    GPIO_PinAFConfig(USART2_GPIO_Port,USART2_GPIO_Pinsource2,USART2_Alternate);
     
    USART_Struct.USART_Mode=((USART_Mode_Rx)|(USART_Mode_Tx));
    USART_Struct.USART_BaudRate=9600;
    USART_Struct.USART_WordLength=USART_WordLength_8b;
    USART_Struct.USART_Parity=USART_Parity_No;
    USART_Struct.USART_StopBits=USART_StopBits_1;
    USART_Struct.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
    USART_Init(USART2,&USART_Struct);
     
     
    USART_ITConfig(USART2,USART_IT_RXNE,ENABLE);
    NVIC_Struct.NVIC_IRQChannel=USART2_IRQn;
    NVIC_Struct.NVIC_IRQChannelCmd=ENABLE;
    NVIC_Struct.NVIC_IRQChannelPriority=0;
    NVIC_EnableIRQ(USART2_IRQn);
    NVIC_Init(&NVIC_Struct);
     
    USART_Cmd(USART2,ENABLE);
/********************************************************************/
     
        /*USART3 Configuration*/
    RCC_AHBPeriphClockCmd(USART3_GPIO_Bus,ENABLE);
    RCC_APB1PeriphClockCmd(USART3_Bus,ENABLE);
     
     
    GPIO_PinAFConfig(USART3_GPIO_Port,USART3_GPIO_Pinsource1,USART3_Alternate);
    GPIO_PinAFConfig(USART3_GPIO_Port,USART3_GPIO_Pinsource2,USART3_Alternate);
     
     
     
    GPIO_Struct.GPIO_Pin=((USART3_Pin_Tx)|(USART3_Pin_Rx));
    GPIO_Struct.GPIO_Mode=GPIO_Mode_AF;
    GPIO_Struct.GPIO_OType=GPIO_OType_PP;
    GPIO_Struct.GPIO_PuPd=GPIO_PuPd_UP;
    GPIO_Struct.GPIO_Speed=GPIO_Speed_50MHz;
    GPIO_Init(USART3_GPIO_Port,&GPIO_Struct);
     
     
    USART_Struct.USART_Mode=(USART_Mode_Rx|USART_Mode_Tx);
    USART_Struct.USART_BaudRate=9600;
    USART_Struct.USART_WordLength=USART_WordLength_8b;
    USART_Struct.USART_Parity=USART_Parity_No;
    USART_Struct.USART_StopBits=USART_StopBits_1;
    USART_Struct.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
    USART_Init(USART3,&USART_Struct);
     
    USART_Cmd(USART3,ENABLE);
     
/********************************************************************/
}
 
 
 
/*******************************/
 
void USART1_IRQHandler(void)
{  
     
}
 
void USART2_IRQHandler(void)
{  
    //
}

Outcomes