AnsweredAssumed Answered

Output 48MHz system clock on a GPIO pin other than MCO pin

Question asked by ER on Jan 3, 2016
Latest reply on Jan 4, 2016 by Clive One
I want to output the max 48MHz clock signal on STM32F030 to drive another subcircuit. The problem is the chip STM32030F4P6 (TSSOP-20 package) I prefer to use doesn't have the MCO pin (PA8). So I have 2 questions:

1. Can this 48MHz signal be produced on another GPIO pin other than MCO pin?  

2. I cannot find the limitations of using 48MHz signal (like load impedance, max driving current, etc.). Where can I find the information? 

Outcomes