AnsweredAssumed Answered

display driver

Question asked by McC.Joe on Jan 3, 2016
Latest reply on Jan 3, 2016 by Clive One
I have the nucleo board and an add-on board with a 2x12 oled character display. Writing to the display is not straight forward because D7..D0 lines are connected to pins on different  ports (PA,PB,PC).
 
Is there a way to structure this hardware so I can write clean C code? 
For instance RS is PB3, WR is PC1, Enable is PA10, D7 is PA8, D6 is PB10, D5 is PB4, D4 is PB5, D3 is PA9, D2 is PC7, D1 is PA3, D0 is PA2. 

Thanks

Outcomes