AnsweredAssumed Answered

STM32Cube bugs?

Question asked by breukers.ron on Apr 19, 2014
Latest reply on May 22, 2015 by mcwiggin.patrick
I started using the STM32Cube using for now the STM32F401 discovery board and Keil software. I like the setup very much as it can make initialization a breeze.
However I have a few comments(bugs?).
- If I use the FREERTOS, and I try to compile the code it comes with the error "freeRtosTest Configuration\freeRtosTest Configuration.axf: Error: L6218E: Undefined symbol xQueueGiveMutexRecursive (referred from cmsis_os.o)." I have to comment out the line 444, 491,494 and 532  of queue.c.
- In the configuration of the target options it always reverts to JTAG mode under debug-settings
- The most problems come from the RTC module. I made a small test program with flashing LEDs to test the RTOS setup. It all works until I enable the RTC module. In the debugger I found that the system hangs at the HAL-RTC-Init instruction. I configured the RTC clock using the LSI.
My question is if I made somewhere a mistake in the STM32Cube setup or if anyone else has the same problem.

Outcomes