AnsweredAssumed Answered

Unable to configure SPWF01SA21 (FW3.4) to communicate directly with a smartphone

Question asked by ferrari.fabrizio on Sep 28, 2015
Latest reply on Oct 5, 2015 by KUMAR.NANDEESH
Goodmorning, 
We bought the STEVAL-IDW001V1 evaluation board and the STEVAL-PCC018V1 module to connect it to the pc; the STEVAL-IDW001V1 it's already updated to the last release FW 3.4.
We need to receive some data from a smartphone on a microcontroller connected to the wifi module, the SPWF01SA shall be the server and it shall create a local network to which 
any smartphone (IOS, Android, Windows) can connect.
The SPWF01SA should open a socket (UDP or TCP) on a port already defined and by our app the smartphone should send data to the module.
The SPWF01SA should in turn send this data (max 10 byte) to the microcontroller via UART. The smartphone should recognize the network, connect to it, open the tansmission and send data.
Is there a SPWF01SA configuration to do this? Is there also an example of instruction which will make thi configuration easier to me?

Outcomes