AnsweredAssumed Answered

STM32F40G-EVAL Ethernet Lwip IAP application

Question asked by bhatia.karan on Oct 30, 2015
Latest reply on Oct 30, 2015 by Clive One
Hello,
I am trying to implement the LWIP_IAP application on the STM32f40g EVAL board. After compiling the project, the program size turns out to be as follows.
Program Size: Code=28150 RO-data=3114 RW-data=260 ZI-data=43612 

I have attached the map file for reference.
1.What should I define my
"USER_FLASH_FIRST_PAGE_ADDRESS" in the main.h file. I have defined it as

0x08060000 currently, is that correct? or do I need to define something else?
2.Also, I have used all the default jumper settings, so I am currently using MII mode. If, I want to use RMII mode, do I need to make some software changes?

 Please help!

Attachments

Outcomes