AnsweredAssumed Answered

Keil 5.16a - STM32F103C8 debugging issue (cannot connect the target)

Question asked by Bogdan Golab on Oct 28, 2015
Latest reply on Nov 5, 2015 by Bogdan Golab
Hi,
I've being using Keil for a few years. I have no issues with debugging when Standard Peripheral Library is used on the same core and same st-link device.
===
I wanted to play with Cubex and HAL and noticed that as long has HAL_init() is used I am experiencing ST-link issues when I want to debug the app. I get 'Cannot connect to the target' error. The ST-Link firmware is up-to-date. There is no problem when SPL is used for the same purpose.
The application is very simple - just blinking (I wanted to start using the HAL drivers).

Does anyone have similar issues?

Thanks,
Bogdan

Outcomes