AnsweredAssumed Answered

Pairing BlueNRG with Android

Question asked by close.nick on May 30, 2016
Latest reply on Dec 1, 2016 by mazzella.damiano
I have our BlueNRG device set up to use a fixed pin for pairing.
I am able to successfully pair with Apple iOS decvices and windows phone when I enter the correct PIN when prompted by the device.
However when connecting to an Android device, the pairing always fails even though I enter the correct PIN when prompted. Using a packet sniffer I can see that the reason for failing is 0x04 (The confirm value does not match the calculated compare value).
I have tried with several different Android devices and versions including 4.4, 5.1 & 6.0 and I have the same issue with all of these.

Has anyone successfully paired an Android device with BlueNRG using a PIN code?

Regards
Nick

Outcomes