AnsweredAssumed Answered

STM32_TDES_ECB_Encrypt

Question asked by pipon.herve.001 on Sep 29, 2015
Latest reply on Sep 30, 2015 by Clive One
Hello,
I want to use STM32CubeExpansion_FwCryptographic_V3.0.0.
In my code I do some test calling STM32_TDES_ECB_Encrypt function

InputMessage = 9E 42 7D 2E 14 C9 83 23
InputMessageLength = 8
TDES_Key = D0 D1 D2 D3 D4 D5 D6 D7 D8 D9 DA DB DC DD DE DF 00 00 00 00 00 00 00 00
I got
OutputMessage = 00 B8 20 5E B2 AD D1 1C
OutputMessageLength = 8

I then want to check it with  http://tripledes.online-domain-tools.com/
and the result is different ....36 f9 12 61 fc 88 d3 0d

I thought they had to be identical : am I wrong?

Regards

Outcomes