AnsweredAssumed Answered

rtc bug stm32 cube l0

Question asked by jesse pinkman on Sep 17, 2015
Latest reply on Sep 17, 2015 by waclawek.jan
Hello,

I have implemented RTC on STM32l053-Nucleo using CubeMX and CubeL0 HAL libraries. I set and get the time and date in RTC using HAL functions but the RTC is not running, I am getting the same time and date I have set. The crystal oscillator connected to RTC as showed in CubeMX is LSI. My IDE is Keil MDK-5. I have posted my RTC initialization function and main function below (main.c is attached).

/****************************** RTC init function **********************/

void MX_RTC_Init(void)
{
    /**Initialize RTC and set the Time and Date
    */
  hrtc.Instance = RTC;
  hrtc.Init.HourFormat = RTC_HOURFORMAT_12;
  hrtc.Init.AsynchPrediv= 127;
  hrtc.Init.SynchPrediv= 255;
  hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
  hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_PC13;
  hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
  hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
  HAL_RTC_Init(&hrtc);
}

**********************MAIN FUNCTION********************

int main(void)
{
  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* Configure the system clock */
  SystemClock_Config();

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_RTC_Init();
  MX_USART2_UART_Init();
/***********************RTC*********************/
    RTC_TimeTypeDef sTime;
  RTC_DateTypeDef sDate;
  RTC_AlarmTypeDef sAlarm;
    
        
  sTime.Hours = 9;
  sTime.Minutes = 30;
  sTime.Seconds = 0;
  sTime.SubSeconds = 0;
  sTime.TimeFormat = RTC_HOURFORMAT12_AM;
  sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sTime.StoreOperation = RTC_STOREOPERATION_RESET;
  HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BCD);

  sDate.WeekDay = RTC_WEEKDAY_MONDAY;
  sDate.Month = RTC_MONTH_AUGUST;
  sDate.Date = 24;
  sDate.Year = 15;
  HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BCD);

    /**Enable the Alarm A
    */
  sAlarm.AlarmTime.Hours = 0;
  sAlarm.AlarmTime.Minutes = 0;
  sAlarm.AlarmTime.Seconds = 0;
  sAlarm.AlarmTime.SubSeconds = 0;
  sAlarm.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;
  sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
  sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
  sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
  sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
  sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
  sAlarm.AlarmDateWeekDay = 1;
  sAlarm.Alarm = RTC_ALARM_A;
  HAL_RTC_SetAlarm(&hrtc, &sAlarm, FORMAT_BCD);
    
    RTC_TimeTypeDef gTime;
    char str[100];
    
  while (1)
  {
        HAL_RTC_GetTime(&hrtc, &gTime, FORMAT_BCD);
        
        sprintf(str, "Time -> %d:%d:%d (sub seconds: %d)\n",sTime.Hours, sTime.Minutes, sTime.Seconds, sTime.SubSeconds);
        HAL_UART_Transmit(&huart2, str, 100, 5000);
        HAL_Delay(1000);
  }

}

Outcomes