AnsweredAssumed Answered

External Loaders for ST-Link V2

Question asked by dickinson.lee.001 on Sep 10, 2015
Latest reply on Sep 11, 2015 by Clive One
I'm looking for a good source of either developed external loaders for the ST-Link V2 or a good reference on modifying the existing loaders that come with the ST-Link utility, I am trying to program a NOR flash (N25Q032A11EF6) attached to a STM32F405RGT6 or a STM32F401RET6. Can anyone help? Thanks. 

Ultimately the goal is to be able to individually address 10 different ST-Link V2s (I need to be able to use the command line interface to select a unique programmer based on the serial number) to program 10 units nearly simultaneously. The way I am currently programming the external memory is with a program loaded to the STM32 through a make file that is part of the WICED SDK, which has config files to be able to use the ST-Link, a Olimex, etc. 

Outcomes