AnsweredAssumed Answered

Ultrasonic receiver

Question asked by stone.jorge on Sep 8, 2015
Latest reply on Sep 8, 2015 by Clive One
Hi,
I made a project with stm32f4-disco that basically receives ultrasonic pulses and it calculates a distance.

It does the following: get values from ADC, fills a buffer, makes some calculations and then sends the result to the computer via serial port.

I would like to repeat this process even if it finishes to do the calculations or not. So for instance, I want to repeat this every 30 ms, the buffer is filled in 25 ms and then begin the calculations. It doesn't matter if it can finish that I would like to fill the buffer again with new values at milisecond 30 and so on. How can I do this?

Here is the code:
// ADC Mesures a 200 KHz (PC.1) STM32F4 Discovery
 
// Assumptions per system_stm32f4xx.c CPU @ 168 MHz, APB2 @ 84 MHz (/2), APB1 @ 42 MHz (/4)
 
// USART TX->PB6 RX->PB7 amb baud rate a 9600
 
#include "stm32f4xx.h"
#include "stm32f4xx_rcc.h"
#include "stm32f4xx_gpio.h"
#include "stm32f4xx_adc.h"
#include "stm32f4xx_dma.h"
#include "stm32f4_discovery.h"
#include "stm32f4xx_tim.h"
#include "stm32f4xx_usart.h"
#include "misc.h"
#include "stdio.h"
 
 
 
void ClockSetUp(void) {
//  Initialize system
    SystemInit();
    RCC_DeInit();
//  PLL Setup
    RCC_HSEConfig(RCC_HSE_ON);
    RCC_WaitForHSEStartUp();
    RCC_PLLConfig(RCC_PLLSource_HSE,5,210,2,4);
    RCC_PLLCmd(ENABLE);
    while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) != SET);
    RCC_HCLKConfig(RCC_SYSCLK_Div1);
    RCC_PCLK1Config(RCC_HCLK_Div4);
    RCC_PCLK2Config(RCC_HCLK_Div2);
    RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
}
 
 
/**************************************************************************/
 
void RCC_Configuration(void)
{
  /* GPIOA clock enable */
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
 
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
 
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
 
 
}
 
/**************************************************************************/
 
void NVIC_Configuration(void)
{
  NVIC_InitTypeDef NVIC_InitStructure;
 
 
  /* Enable the DMA Stream IRQ Channel */
  NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream0_IRQn;
  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);
 
 
  NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
  NVIC_Init(&NVIC_InitStructure);
 
}
 
/**************************************************************************/
 
void GPIO_Configuration(void)
{
  GPIO_InitTypeDef GPIO_InitStructure;
 
  /* ADC Channel 11 -> PC1 */
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
 
  /* USART TX->PB6 RX->PB7 */
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
  GPIO_Init(GPIOB, &GPIO_InitStructure);
 
  /* Connect TIM13 pins to AF */
  GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM13);
 
  /*Connect PB6 and PB8 to AF*/
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_USART1);
  GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_USART1);
 
 
}
 
/**************************************************************************************/
 
void ADC_Configuration(void)
{
  ADC_CommonInitTypeDef ADC_CommonInitStructure;
  ADC_InitTypeDef ADC_InitStructure;
 
  /* ADC Common Init */
  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
  ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
  ADC_CommonInit(&ADC_CommonInitStructure);
 
  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
  ADC_InitStructure.ADC_ScanConvMode = DISABLE; // 1 Channel
  ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; // Conversions Triggered
  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;
  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T2_TRGO;
  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
  ADC_InitStructure.ADC_NbrOfConversion = 1;
  ADC_Init(ADC1, &ADC_InitStructure);
 
  /* ADC1 regular channel 11 configuration */
  ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 1, ADC_SampleTime_15Cycles); // PC1
 
  /* Enable DMA request after last transfer (Single-ADC mode) */
  ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
 
  /* Enable ADC1 DMA */
  ADC_DMACmd(ADC1, ENABLE);
 
  /* Enable ADC1 */
  ADC_Cmd(ADC1, ENABLE);
}
 
/**************************************************************************************/
 
#define BUFFERSIZE 5000
 
__IO uint16_t ADCConvertedValues[BUFFERSIZE];
 
static void DMA_Configuration(void)
{
  DMA_InitTypeDef DMA_InitStructure;
 
  DMA_InitStructure.DMA_Channel = DMA_Channel_0;
  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0];
  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
  DMA_InitStructure.DMA_BufferSize = BUFFERSIZE; // Count of 16-bit words
  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
  DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;
  DMA_InitStructure.DMA_Priority = DMA_Priority_High;
  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
  DMA_Init(DMA2_Stream0, &DMA_InitStructure);
 
  /* Enable DMA Stream Half / Transfer Complete interrupt */
  DMA_ITConfig(DMA2_Stream0, DMA_IT_TC | DMA_IT_HT, ENABLE);
 
  /* DMA2_Stream0 enable */
  DMA_Cmd(DMA2_Stream0, ENABLE);
}
 
/**************************************************************************************/
 
void TIM2_Configuration(void)
{
  TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
 
  /* Time base configuration */
  TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
  TIM_TimeBaseStructure.TIM_Period = (84000000 /200000) - 1; // 200 KHz, from 84 MHz TIM2CLK (ie APB1 = HCLK/4, TIM2CLK = HCLK/2)
  TIM_TimeBaseStructure.TIM_Prescaler = 0;
  TIM_TimeBaseStructure.TIM_ClockDivision = 0;
  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
 
  /* TIM2 TRGO selection */
  TIM_SelectOutputTrigger(TIM2, TIM_TRGOSource_Update); // ADC_ExternalTrigConv_T2_TRGO
 
  /* TIM2 enable counter */
  TIM_Cmd(TIM2, ENABLE);
}
 
/**************************************************************************************/
 
void DMA2_Stream0_IRQHandler(void) // Called at 1 KHz for 200 KHz sample rate, LED Toggles at 500 Hz
{
  /* Test on DMA Stream Half Transfer interrupt */
 
  if(DMA_GetITStatus(DMA2_Stream0, DMA_IT_HTIF0))
  {
    /* Clear DMA Stream Half Transfer interrupt pending bit */
 
    DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_HTIF0);
 
    /* Turn LED3 off: Half Transfer */
    STM_EVAL_LEDOff(LED3);
 
    // Add code here to process first half of buffer (ping)
 
  }
 
  /* Test on DMA Stream Transfer Complete interrupt */
  if(DMA_GetITStatus(DMA2_Stream0, DMA_IT_TCIF0))
  {
    /* Clear DMA Stream Transfer Complete interrupt pending bit */
    DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_TCIF0);
 
    /* Turn LED3 on: End of Transfer */
    STM_EVAL_LEDOn(LED3);
 
    // Add code here to process second half of buffer (pong)
 
  }
}
/**************************************************************************/
 
void USART_Configuration(void){
 
    USART_InitTypeDef USART_InitStruct;
 
    USART_InitStruct.USART_BaudRate = 9600;
    USART_InitStruct.USART_WordLength = USART_WordLength_8b;// we want the data frame size to be 8 bits (standard)
    USART_InitStruct.USART_StopBits = USART_StopBits_1;     // we want 1 stop bit (standard)
    USART_InitStruct.USART_Parity = USART_Parity_No;        // we don't want a parity bit (standard)
    USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // we don't want flow control (standard)
    USART_InitStruct.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; // we want to enable the transmitter and the receiver
    USART_Init(USART1, &USART_InitStruct);                  // again all the properties are passed to the USART_Init function which takes care of all the bit setting
 
    USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1 receive interrupt
 
    USART_Cmd(USART1, ENABLE);
 
}
 
/**************************************************************************/
 
void USART_puts(USART_TypeDef* USARTx, volatile char *s){
 
    while(*s){
        // wait until data register is empty
        while( !(USARTx->SR & 0x00000040) );
        USART_SendData(USARTx, *s);
        *s++;
    }
}
 
/**************************************************************************/
 
// this is the interrupt request handler (IRQ) for ALL USART1 interrupts
void USART1_IRQHandler(void){
 
    // check if the USART1 receive interrupt flag was set
    if( USART_GetITStatus(USART1, USART_IT_RXNE) ){
 
        static uint8_t cnt = 0; // this counter is used to determine the string length
        char t = USART1->DR; // the character from the USART1 data register is saved in t
 
        /* check if the received character is not the LF character (used to determine end of string)
         * or the if the maximum string length has been been reached
         */
        if( (t != '\n') && (cnt < MAX_STRLEN) ){
            received_string[cnt] = t;
            cnt++;
        }
        else{ // otherwise reset the character counter and print the received string
            cnt = 0;
            USART_puts(USART1, received_string);
        }
    }
}
 
/**************************************************************************************/
 
int main(void)
{
  ClockSetUp();
 
  RCC_Configuration();
 
  NVIC_Configuration();
 
  GPIO_Configuration();
 
  USART_Configuration();
 
  TIM13_Configuration();
 
  TIM2_Configuration();
 
  DMA_Configuration();
 
  ADC_Configuration();
 
  /* Start ADC1 Software Conversion */
  ADC_SoftwareStartConv(ADC1);
 
  int i=0;
  int value;
  int valueinmV;
  char strvalue [20];
  float temps;
  float distancia;
 
 while (i<BUFFERSIZE){
        value=ADCConvertedValues[i];
        valueinmV=(value*3000)/4095; //conversion a mV
 
        if (valueinmV>2000){
            temps=i/200000.;
            distancia=temps*340;
            sprintf(strvalue, "Distance is %f\r\n", distancia);
            USART_puts(USART1, strvalue);
            break;
        }
 
        i=i+1;
 
 
while(1){
 
    }
 
}

Thank you for reply

Outcomes