AnsweredAssumed Answered

[solved]STM32F7 NOR memory with FMC

Question asked by mszal.rafal on Sep 7, 2015
Latest reply on Dec 22, 2015 by teal.andy
Hello,
I have some problems with FMC when I try to port my code from SMT32F407(with FSMC interface) to new project based on STM32F746(with FMC). The only changes I've made are timings(adapted to 216 MHz clock) and init structures(FSMC => FMC).
I have also SRAM connected to the same data and address bus and it works well, so I think that my hardware is ok and problem is inside init code.
Thus, I have few questions: is there any difference between using FMC on STM32F4 and STM32F7? Should I change or add something in initialisation code when using FMC on STM32F7?

Outcomes