AnsweredAssumed Answered

STM32F107VCT6 - programming via USART1

Question asked by rybicki.tomasz on Sep 4, 2015
Latest reply on Sep 6, 2015 by rybicki.tomasz
Dears,

I've got Core107V board from Waveshare with STM32F107VCT6 (rev.Z) and I want to flash my program using USART1.

I've plugged FTDI converter the board according to the information in datasheet.


3.3V => 3.3V on Core107V
GND => GND on Core107V
TX => PA10
RX => PA9

BOOT0 and BOOT1 are set correctly for sure.

I've used standard setting in ST Downloader Demo, Baud: 115200, Parity Even, timing 5, data bits 8.

Unfortunately ST Downloader says it cannot connect to the board (No response from target).

Could u pls give me any advice how to get it connected?

Please see the board:
http://www.wvshare.com/img/devkit/Core107V/Core107V-intro-1.jpg

Regards,
Tomek

Outcomes