AnsweredAssumed Answered

Consuming Kiel library file .Lib into application Keil project

Question asked by Reddy.Harinadha on Aug 31, 2015
Latest reply on Sep 1, 2015 by Reddy.Harinadha
Hello Dears,
I use stm32f103ve. Flash range is 0x08000000 ->0x08080000
I have 3 projects.
1. Simple bootloader application which is located (start= 0x08000000,  size =0x80000)
2. An library project in which the settings are set (start= 0x08002000,  size =0x80000)
3. An application proj which will consume .lib has settings (start= 0x08002000,  size =0x80000)
 
Is this correct ? or the size of memory should be set to 0x7E000 ?
And coming to the next point,
I Added .lib to application project, links without any errors, flashing also ok. But unable to access the MCU for debugging, just after executing the clocks configuration.
( There is nothing wrong with the code except linking, because before making the application project code into library and application projects, it works fine)
I feel that the linking of .lib to application project is not being done properly. 
I'm very new to the .lib & linking in the Keil. Pls help.

Outcomes