AnsweredAssumed Answered

UDP packet receive problem

Question asked by khoshnoud.borzoo on Aug 24, 2015
Latest reply on Jun 14, 2016 by Odry.Akos
Hi all,
I'm using UDP Echo client code example in STM32F217xx.I can send the custom buffer...ok but I can't receive udp packets from PC.
I have a VS code that can generate UDP test packets as well...

I use the udp_recv function that sets a call back function...I have a breakpoint in callback function...but no packet receive.
When I check in wireshark, it says: destination port is unreachable !!! I changed the port but the problem remains...

It would be appreciated if you help any way.Thanks

Outcomes