AnsweredAssumed Answered

STM32 discovery board console Port driver

Question asked by athukuri.ashok on Aug 21, 2015
Hello All,

I started working/learning micripython using STM32F407 discovery board. The board I'm using is already with micropython (as my colleague used it earlier).


I connected board to Windows PC and in ST Link utility I see this:
12:24:40 : ST-LINK SN : 55FF72065075495446332087
12:24:40 : ST-LINK Firmware version : V2J23S0
12:24:40 : Connected via SWD.
12:24:40 : SWD Frequency = 1,8 MHz.
12:24:40 : Connection mode : Normal.
12:24:40 : Debug in Low Power mode enabled.


and Colored LEDs are blinking, Now I want to run few micropython commands on board. 
I connected a different USB cable at CN5 and I don't see any COM port in device manager in windows. Need help.


As of now I don't have a Linux PC to flash new binary on to the board, that's the reason I'm trying on Windows PC


Thanks
 

Outcomes