AnsweredAssumed Answered

Sampling USB interrupt pin

Question asked by Nayani.Partha on Jul 27, 2015
Latest reply on Jul 28, 2015 by Nayani.Partha
Hi all,
In STM32 USB device, there is an internally connected EXTI_Line18 for USB interrupt. When USB is connected to HOST, an interrupt is generated on this line. Is there a way of sampling the status of this line? I would like to monitor this as gpio input and see if it is in high or low state. Can this be done? If yes, which port is this i/o connected to? Thank you.

Outcomes