AnsweredAssumed Answered

Example program requires NOR flash binary to be written first

Question asked by olson.gary.001 on Jul 26, 2015
Latest reply on Jul 26, 2015 by Clive One
Hi,
  I have a STM3210E_EVAL board and I have been going through most of the example programs.  There is one example program with the name:FSMC_NOR_CodeExecute.

If I run this program it will cause a Hard Fault condition because the program is trying to execute code in the nor flash that has not been written yet.  The readme file says I am supposed to program the nor flash at 

Program the NOR memory with the example provided in the "binary" directory
@note You can use ST-LINK v3.4.6 tool and select NOR Flash memory in the external loader and
      then flash the binary file at @0x64000000.

Is it possible to use a ULINK2 and keil to program the nor flash.

I found the GPIO_toggle.bin file in the binary directory.


The second step is to download the main program to run the nor flash program.

Thanks,
  Gary 








Outcomes