AnsweredAssumed Answered

Configuration of SWD frequency with ST-LINK_CLI

Question asked by Julian on Jul 23, 2015
Latest reply on Jul 23, 2015 by Julian
Hello all,

i'm using the ST-LINK_CLI to flash software on an STM32F429 with 2MB Flash. In order to increase the speed, I'd like to configure the SWD frequency to the maximum (AFAIK 4MHz at the moment). I can do this configuration with the ST-Link Utility (GUI), but I didn't find any command line parameters in the "ST-LINK Utility software description (UM0892)" for the configuration of the frequency.

Is this feature not documented or not implemented?

regards
Julian

Outcomes