AnsweredAssumed Answered

Input capture timer - measure frequency

Question asked by Saphymoo on Jul 20, 2015
Latest reply on Jul 21, 2015 by Saphymoo
Hi, I had to measure frequency but in a large range of frequency.
the target is a STM32L053.
I would like to realize something like :
T2 generate a 10hz signal on PA0(using internal clock, and compare/match)
wiring this signal to T21 Capture source PA2 (both edge),
while T21 used external clock as input on PA1.
Capture should set Interrupt to compute frequency.

Is this possible ?
All try I maid with STM32CubeMx fail.
Have you an idea to help me ?

Best regards,
Saphymoo.

Outcomes