AnsweredAssumed Answered

Program runs correctly in step by step debug but not in run

Question asked by kasapoglu.orkun on Jul 16, 2015
Latest reply on Jul 16, 2015 by kasapoglu.orkun
Hi. I'm using stm32f429i-discovery I am controlling RFM69HC module (device) over SPI and I could get communicating both of them. I'm checking device's ID, and some other controllable registers and there is no problem of these. I've created a device struct and creating some arrays dynamcally so first I needed more heap size then the default one (in the *.s file Heap_Size variable) and increased it to 400 (default is 200). Now I am facing an error that when I connecting the board with keil and run without any breakpoints, program has not set some registers in the device over spi (I'm checking written value with reading the same address on the device), and returning (-1) but when I put there a bp then go into the function and complete it step by step, it is not returning any error (which means returns 0) device is configuring correctly. I'm checking these return values and writing the results to the LCD on discovery board. When I stepping function returning 0, when in run it's returning -1. I'm thinking about memory alignment but I'm not sure.

Outcomes