AnsweredAssumed Answered

problem in sending data with nrf24l01+ Module stm32F030F4 microcontroller

Question asked by rajabniya.reza on Jul 10, 2015
hello everybody
I want to transmit data with NRF24L01+. I use two boards that are based on two stm32F030F4 Microelectronics.
I attached my code. when i press a bottom that connected to PA14, it should send 0x0002, and LED that connected to PA0 on receiver board
 should be turn on, but when i check SPI received data on receiver board,  with "if(SPI_ReceiveData8(SPI1)==0x0002)", noting happened. please help me

Attachments

Outcomes